AThere are no laws that regulate the “sound volume” of aerial ultrasonic waves. As a general guideline, it is reported that long exposure to ultrasounds of 105-115dB or more may cause buzzing in the ear and discomfort. It is recommended that the ultrasonic volume be kept below the above limit in the sensor range used.