PTC Thermistors (POSISTOR) FAQQ[PRF Series] What is the difference between sensing temperature 1 and sensing temperature 2 in PRF series.

A

The sensing temperature 1 is 10 times the initial resistance, and the sensing temperature 2 is 100 times the initial resistance. Sensing temperature 2 (100 times) can be used to increase the difference of output voltage between normal and detected temperatures, or to detect temperatures in multiple series connections.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.