Electrical Double-Layer Capacitors with Long Life, High-Temp Reliability Deliver Advanced Solution

DMT Series

9/9/2013

Smyrna, GA, Sep 9, 2013 - Murata Americas today announced the launch of its DMT series, one of the most reliable electrical double-layer capacitors (EDLC) available on the market today. The solution offers superior long-term, high temperature reliability (five years at 70º C), a maximum operating temperature of 85º C, low resistance (130mΩ of high-current, high-output charging and discharging), a nominal capacitance range of 470mF, and an innovative design that enables high voltage handling (4.2V). Measuring 14x21mm with a thickness of just 3.5mm, the DMT series is ideally suited for applications such as solid state drive (SSD) and communication system backup, power assistance for smart meters, and energy-harvesting devices.

The expansion of these markets is driving the demand for smaller, thinner, and low-resistance capacitors that assure high reliability in the event of power failures. For example, since an increasing number of end products are being used outdoors (e.g., smart meters), there is a heightened focus on ensuring that solutions have exceptional dependability. Coupled with more miniaturized features, design engineers now require products that are both extremely advanced and eco-friendly.

“To develop solutions with unprecedented reliability, functionality, and efficiency, Murata is continually pushing the envelope with our research and development efforts,” said Mark Waugh, Business Development Manager, Murata Americas. “The launch of the DMT line and the class-leading features that it incorporates exemplifies our ability to deliver leading-edge supercapacitor technology.”

The basis behind this technology is the result of the company’s collaboration with CAP-XX. In order to meet demand for devices with greater efficiency and functionality, Murata strategically acquired supercap technology from CAP-XX in 2008. Murata’s focus on EDLC research and development, coupled with CAP-XX’s market expertise, drives the advancement of enhanced EDLC design.

Samples of the DMT series are now available, with leadtimes up to 8 weeks for production quantities. More information about this product, as well as other EDLC solutions from Murata, can be found at www.murataamericas.com/edlc.


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com