Murata introduces 0805-size baluns for smart phone NFC circuits

DXW21BN2511N

6/5/2017

Overview

Murata Manufacturing Co., Ltd., has started commercially manufacturing the "DXW21BN2511N" balun for NFC*1  circuits for smart phones and other compact devices. This new product has been in production since February 2017.

  

Supplementary notes

The short-range communications market is in a state of disarray, with different communications standards such as "Felica" in use in "Osaifu-Keitai" (mobile phone with wallet functions) and other services in Japan and "MIFARE*2 " used on short-range IC cards overseas. The new international standard NFC (13.56 MHz) has been established to ensure compatibility with each of the standards. Because of this, in recent years the NFC standard has been progressively adopted for smart phones, tablet computers, laptop computers, wearable devices, and other compact device equipment.

A balun is used in these NFC circuits for signal conversion (balanced-unbalanced signal conversion). Murata Manufacturing has started commercially manufacturing the 0805 inch size (2.0 x 1.2 mm) balun "DXW21BN2511N," which has the input port impedance of 25Ω that is currently required in the market.

  

Product site URL

DXW21BN2511N□
For product details, click here.

  

Terminology

*1 NFC: Near Field Communication
*2 MIFARE: A technology used for contactless/short-range type IC cards



Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com