The World's Smallest! Development and Starting Expanded Sales of a Micro DC-DC Converter

The World's Smallest! Development and Starting Expanded Sales of a Micro DC-DC Converter

2/15/2012

Murata Manufacturing Co., Ltd.

President/ Statutory Representative Director: Tsuneo Murata

Production of this product has stopped.
Contact Murata for inventory availability and
possible alternative products.

Overview

Murata Manufacturing Co., Ltd. has successfully developed the world's smallest micro DC-DC converter.*
The line-up has been expanded to include four series; expanded sales have been started.
Furthermore, some series are already installed in SmartPhones.

*Refers to LXDC2UR series: 2.5 mm x 2.3 mm (supports up to 0.6 A) ; LXDC3EP series: 3.5 mm x 3.2 mm (supports up to 1.0 A) .

Comment from Executive Vice President Technology & Business Development Unit Member of the Board of Directors Hideharu Ieki

The micro DC-DC converter features ultra-compact size and suppression of EMI noise. We are certain that this converter will greatly contribute to miniaturizing mobile devices while they continue to provide even greater functionality.

Features

  1. Achieved a ferrite substrate with an embedded inductor and EMI filter feature by combining areas of engineering for materials, multi-layer processing, and circuit design that we have developed over the years.
  2. Achieved the world's smallest sizes by mounting a power IC and I/O capacitor to a ferrite substrate.
    (LXDC2UR series; LXDC3EP series)
  3. Achieved the shortest wiring by integrating the power IC and inductor.
  4. Embedded an EMI suppression filter; reduced harmonic noise.

    Embedded an EMI suppression filter; reduced harmonic noise.

  5. Supports up to a maximum load current of 3.0A (on the LXDC55B series)
  6. Supports voltage step-up (on the LXDC44A series)

Background

As electronic devices have increasingly powerful functionality, it has become necessary to supply power individually over each feature circuit. To support needs in the marketplace, we have successfully developed and commercialized for the first time, in October 2010, a micro DC-DC converter. Our success is the result of applying our unique circuit design engineering and multi-layer processing engineering. Marketplace needs include:

  1. Reduced component surface mount area;
  2. Suppressed EMI noise; and
  3. Energy conservation.

Currently, we are providing a line-up that includes a total of four series to start expanding sales. These series include the world's smallest devices that support even further miniaturization, high-current components that handle up to 3.0A, and voltage step-up types. We will continue to work on developing products that are ultra-compact, and have low EMI noise, to contribute to optimization of power-surrounding circuit designs.

Applications

All mobile devices such as SmartPhones and the like.

Part Number

Series Name Type Size Capacity External View
LXDC2UR
Series
Voltage
step-down type
World's Smallest!
2.5 x 2.3mm
0.6A
LXDC2UR Series
LXDC3EP
Series
Voltage
step-down type
World's Smallest!
3.5 x 3.2mm
1.0A
LXDC3EP Series
LXDC55B
Series
Voltage
step-down type
5.7 x 5.0mm Supports High Currents!
3.0A
LXDC55B Series
LXDC44A
Series
Voltage
step-up type
4.0 x 4.0mm 0.7A
LXDC44A Series

Characteristics

See the Selection Guide of Micro DC-DC Converters.

Production

Starting mass production sequentially at Okayama Murata Manufacturing Co., Ltd. from October 2011.

Patent Information

3 patents granted
5 patents pending


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com