In collaboration with lighting equipment makers, we developed a lighting control system that can adjust the intensity and color of interior light. It creates a pleasant interior space and contributes toward energy-saving lifestyles.
Most characteristic of the system is a wireless communication network connecting the gateway (base) and the light fixtures (devices) . One can change the layout of the fixtures or replace them without any constraints on wiring for network connection. The system allows free rearrangement of the fixtures.
The system is capable of adjusting the light fixtures individually or collectively in a group, which allows users to choose the appropriate brightness that serves its purpose for a space. Users can adjust the setting using their mobile devices such as tablet computers. The scheduler provides scene control, allowing automatic adjustment in response to the intensity of outdoor natural light (reducing brightness inside) , or automatically switching off the lights at the preset closing time of facilities. These functions contribute toward energy-saving lifestyles.