Sound Components (Buzzer)Basics and Technical Terms of Sound Components

What Is a Sound Component (Acoustic Component)?

What is sound?

Sound is a vibration of air.

Examples) Security buzzer, fire-alarm device and alarm clock etc.

Image of Sound Sound source pushes air → Atmospheric pressure changes (sound waves) → Vibration of the eardrum → The vibration is perceived as sound

Air pressure is called Sound Pressure when a sound is propagated through the air.
The number of times of the dilatational wave of air per a second is frequency.

Loudness and pitch of sound

Volume and SPL (Sound Pressure Level)

The SPL indicates the sound volume. The unit is decibel (dB). The higher the SPL, the louder the sound.
Minimal loudness of sound perceived by human is defined as 0dB (20µPa).

Sound pressure that Murata’s sound component produces is approximately 70 to 90dB (measured in 10cm distance). The SPL is about 20 dB for a whisper, about 60 dB for a normal conversation and about 100 dB under the tracks of a train.
The more distant the receiver is from sound source, the lower sound gets. “Specification of Sound Pressure Level”: The necessary information are the distance from the sound source and how loud the sound should be there.

Image of Loudness and pitch of sound

Frequency (Pitch of a sound)

In general, man’s audible frequency range is about 20 Hz to 20 kHz. Especially, the frequency range of 2 kHz to 4 kHz is the most audible. For this reason, the most of piezoelectric sound components are used in this frequency range.

  • *As we get older, it tends to become harder to hear sounds with a high frequency.
Image of Frequency (Pitch of a sound)

What is buzzer?

Buzzer is a component producing sound of alarm and electronic sound.

Examples) Security buzzer, fire-alarm device and alarm clock etc.

Buzzer plays an important part as a man-machine interface. The buzzers which apply piezoelectric ceramics are “Piezoelectric Buzzers”. We generally call “buzzer”, however, a formal name is “piezoelectric sound component”.

What Is a Speaker?

A speaker is a device that converts electrical signals into air vibrations—in other words, it generates sound.
Buzzers and speakers are the same in that they both generate sound. However, they have the following differences.

Buzzers
Used in alarms and warning sounds to generate sounds with a specific frequency
Speaker
Used in music and audio playback to generate sounds with a wide range of frequencies

Technical Terms

What Is a Sound Body?

A sound body refers to an object that generates sound. It is also called a sound source.

Examples) Guitars, buzzers, etc.

What Is a Sound Element?

A sound element refers to an element that vibrates to generate sound.

Examples) Guitar strings, piezoelectric ceramic elements of piezoelectric buzzers, etc.

What Is Sensitivity?

Sensitivity refers to the degree of the response (output) to the input given to a target object.

Examples) SPL sensitivity: Ratio of the output SPL with respect to the input power

What Is Directionality?

Directionality refers to the difference that arises in the volume and SPL of sound depending on the direction when that sound is generated from a sound source.

What Is Frequency Response?

Frequency response refers to the changes in the amplitude and phase of signals output in a steady state with respect to the input signals.

What Is the Sound Frequency?

The phenomenon by which an object starts to vibrate when vibrations with a frequency the same as the natural frequency of each object are applied is called resonance. The frequency at which this resonance occurs is the resonance frequency.
If sound waves with a frequency close to the natural frequency are input to a sound element, the amplitude increases greatly in the acoustic phenomenon. This frequency is the sound frequency.

A piezoelectric buzzer produces a large volume by generating sound waves close to the natural frequency of a resonator (case) with a built-in diaphragm.

Image of Sound Frequency

What Is Impedance?

Impedance is a numerical representation of the difficulty of current flow in an AC circuit. It represents the ratio of voltage and current.

The impedance characteristics of piezoelectric buzzers are shown in the figure on the right. The impedance reaches its minimum value at the resonance frequency.

Figure of Impedance