Supercapacitors(EDLC) FAQ

Configurations/Material

What is the structure of Murata's supercapacitor(EDLC) like?

Murata's supercapcitor(EDLC) consists of electrodes, electrolyte (and electrolyte salt) , and the separator, which prevents facing electrodes from contacting each other. Activated carbon powder is applied to the electricity collector of the electrodes. The electrical double layer is formed on the surface where each powder connects with an electrolyte. 


Structure

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send