Supercapacitors(EDLC) FAQ

Quality/Reliability

What conditions should I store supercapacitors(EDLC)?

Term of warranty for this product is one year after packaging in outer package, under the conditions below with sealed package.
Recommended storage environment:  Room temperature: 30 ºC
Humidity: No more than 60%RH
This product cannot be baked.

Storage conditions after opening outer package.
(1) Term of warranty of this product is three months after opening sealed package.
(2) Please keep product under the following conditions in sealed package.
Temperature: 5-35ºC
Humidity: No more than 70%RH. No condensation.
Avoid any acidic or alkaline environment.
Avoid excessive external force on this product while in storage. 
(3)Please keep product in sealed package before use.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send