Ceramic Capacitors FAQ

Characteristics

What is the difference between operating temperature range and temperature range?

The difference between "operating temperature range" and "temperature range" in the specifications of ceramic capacitors is shown below.

Operating temperature range Temperature range
The temperature range in which the target capacitor can be used continuously according to the design (operating temperature is measured on the surface of the chip). The temperature range in which the target capacitor satisfies the capacitance change ratio or temperature coefficient as the temperature characteristics of the target capacitor.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send