Ceramic Capacitors FAQQ[Temperature characteristics] What is the difference between Murata part number code "B1" and "B3" corresponding to JIS code "B"?

A

The temperature characteristic code "B" specified by JIS can individually specify the capacitance change rate when a voltage is applied.
Murata defines the capacitance change rate when one half of the rated voltage is applied as follows.

B1: within +10%/-30%
B3: No regulation

For more information, see this technical article.

Actual case

img_16.gif

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.