Ceramic Capacitors FAQQWhat is the material of lead type products ?

A

Lead wires consist of CP wires or Cu wires. The construction of each type is shown in the figure below.
The material of the lead wires differs depending upon the product, please contact us for details.

※The molten tin plating contains 1% to 3% copper.

Contact us

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.