Ceramic Capacitors FAQ

Configurations/Material

What kind of material and method do you use for lead type products?

The outermost plated layer consists of tin (Sn).

It is formed by a hot-dip process.

The molten tin plating contains 1% to 3% copper.



<Related article>
Example case how to choose leaded products (wires) and customization

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send