Ceramic Capacitors FAQ

Safety standard

When using Safety Standard Certified products in a DC voltage line, up to what voltage of a line can be used?

Under the safety standards, products can be used with a DC voltage up to the equivalent of the rated voltage. For Murata’s safety standard certified products, the limits are as follows:

Products rated at AC250V → Guaranteed up to DC250V
Products rated at AC300V → Guaranteed up to DC300V

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send