Ceramic Capacitors FAQQAre there any problems in performing manual repair or reworking (replacement, removal ⇒ mounting) of multilayer ceramic capacitors mounted on boards? Are there any points to be aware of when performing manual repair or reworking?

A

When performing manual repair or reworking, it is necessary to pay attention to the following two issues, particularly because of temperature change and residual stress.

1. In order to prevent damage (cracks) to the component caused by localized rapid heating and heat shock, preheat the chip or take other measures to reduce heat shock to the chip.
2. The board temperature is lower than that used for reflow soldering, so a difference in residual stress occurs during cooling, and the mechanical strength (resistance to board bending) tends to decrease. In order to increase the strength, it is necessary to maintain a high board temperature during soldering.

Repair/rework task flow

Repair/rework consists of the following two tasks.
- Removal task: Removing a capacitor mounted on a board
- Mounting task: Mounting a new capacitor

Repair task flow
<Removal task>
1. Coat with flux.
2. Preheat the board.
3. Heat the mounting area to melt the solder.
4. Remove the capacitor.
5. Cool the board.

<Mounting task>
6. Add solder.
7. Position the capacitor on the board.
8. Preheat the board.
9. Heat the mounting area to melt the solder.
10. Cool the board.

* When only mounting capacitors such as when creating product prototypes, perform only the mounting task. In these cases, the solder-adding task consists of coating with solder.

Heating conditions

The figures below show standard temperature profiles (Figure 1, Figure 2). The solder composition is assumed to be Sn-3.0Ag-0.5Cu. Thermocouples are used to measure the temperature on the front and back of the board.

1. Preheat the entire board from the back side for 90 s.
2. Next, heat the area around the mounted component on the front of the board, and also heat from the top and bottom of the board to melt the solder.

The ultimate temperature during heating must be increased in locations where it is particularly difficult for solder to melt, even in a multilayer board (Figure 2).

Temperature measurement method

- Temperature measurement: K thermocouple
- Thermosetting resin: Epoxy resin

The temperature is measured in two locations on the front (the surface the capacitor is mounted on) and back of the board. Position a thermocouple in contact with the board in the center between the lands and fix it in place using thermosetting resin.

Heaters

1. Preheater
The preheater should have a wide heating area and be capable of preheating the entire subject board.

2. Heater
It is recommended to use a spot heater (hot-air heating).
* This is because spot heaters are easily obtained local heating devices.

Points when selecting tools for small components and high-density mounting boards

When handling 0603-size or smaller components and high-density mounting boards, care must also be taken to select the proper tools in addition to the heaters. The following points should be considered when selecting tools for the above tasks.

1. Magnifying device
It is recommended to use a microscope as the magnifying device for the tasks. An area heater is used to preheat the board, so an arm-type stand should be used.

2. Tweezers
When removing a capacitor from a high-density mounted board, it is recommended to use precision tweezers with a tip thickness of 0.1 mm or less to avoid contact with surrounding components.

Repair task procedure

The procedure for repair or reworking of a 0603-size capacitor on a high-density mounted board is described below.

<Capacitor removal process flow>

<Capacitor mounting process flow>

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.