Ceramic Capacitors FAQ

Safety standard

What is the status of the “GA3” (Type GD) “Y3” series, which is a subclass of the “Y” Class capacitors under safety standard IEC60384-14. Since the Safety standard for the “Y3” series, under SEMCO (Sweden) standards has been abolished, will the production of the “GA3 Series (Type GD)” “Y3” capacitors be discontinued?

The expiration date of Type GD / Y3 certified by SEMKO (Sweden) is July 10, 2016.
However type GD series has been certificated not only by SEMKO for Y3 capacitors, but also by UL (United States) for the information appliance standard 60950-1.
We will keep the authorized acquisition of the UL information appliance standard 60950-1, and will continue to manufacture Type GD capacitors under the UL certification only.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send