Polymer Capacitors FAQ

Quality/Reliability

What is the average reel size of the ECAS series?

Case Size D4 (T=1.9mm/size is 3000pcs/reel @ ø 330mm)
Case Size D6 (T=2.8mm/size is 2500pcs/reel @ ø 330mm)
Case Size D9 (T=4.2mm/size is 2000pcs/reel @ ø 330mm)

img_06.gif

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send