Trimmer Capacitors FAQ

Mounting

Which Trimmer Capacitors can be reflow-soldered at a high temperature?

All of Murata's Trimmer Capacitors that are recommended for reflow soldering meet the requirements for high temperature reflow soldering.

 

Pre-heating 150 to 180°C 60 to 120 sec. 
Heating 230°C 30 to 50 sec.
Peak Temperature
260 +5/-0°C
1 sec.
Cycle of reflow
2 time
 

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send