Piezo vibe FAQ

Operating circuit

(Piezo vibe) Is there any way to prevent inrush current?

It can reduce peak current by using LPF. We have confirmed that inrush current of about 16 mA can be reduced to about 6 mA.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send