Piezo vibe FAQ

Characteristics

(Piezo vibe) Why did murata select frequency 240Hz?

To be said Generally,  one of the vibration that is easy to feel by human is 200 to 250 Hz.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send