Piezo vibe FAQ

Characteristics

(Piezo vibe) How much maximum voltage is?

Maximum input voltage of IC is 5V, but input voltage of piezo vibe is defined 3.5V.
Even if more than 3.5 volts are applied, the weight and case will interfere with each other, so quantity of vibration will not increase.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send