Piezo vibe FAQ

Mounting

(Piezo vibe) Is there any recommendation to connect lead wire onto terminal?

We recommend for connecting diameter of 0.3 mm or less lead wire. Since there is a possibility of being damaged characteristic, please solder it without putting the soldering iron for a long time.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send