Piezo vibe FAQ

Mounting

(Piezo vibe) How to mount it on the board?

Please fix it with double-sided tape, then connect the terminal of electrode electrically.
Please apply load at 6 ~ 8 N uniformly.Due to the characteristics of double-sided tape, fixing power will increase by leaving for more than 11 hours after installation.
For electrical connection, prepare lands of the following dimensions on PC board.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send