Acceleration Sensors FAQ

Operating Circuit

Are the SCA610/620 products known to have any EMI emission problems?

Parts are automotive tested and approved. Classification has been done according to CISPR22 class B requirements. The results are on the level of 20dBuV/m with the bandwidth of 100kHz - 1GHz. Our customers have not indicated any EMI problems so far.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send