Acceleration Sensors FAQ

Characteristics

What is non-linearity?

Non-linearity is defined as the deviation of the output from the straight line defined by sensitivity. Non-linearity should not be mixed with the effect of angular mounting errors and cross-axis sensitivity on the sinusoidal behaviour of the accelerometer in the gravitational field.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send