Acceleration Sensors FAQ

Characteristics

When using the SPI to communicate with the inclinometer, what is the maximum sampling rate?

The maximum practical sampling rate is approximately 500 Hz.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send