Acceleration Sensors FAQ

Others

How does the field programmable temperature compensation work?

Please see Technical Note 6. (PDF: 420KB)

Temperature compensation is done internally in the ASIC. The type of compensation is linear and the compensation is calibrated and programmed during factory testing, thus sensor internal temperature compensation is not field programmable. Additional (higher order) temperature compensation can be done by with external compensation by calibrating sensor behavior at system level.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send