AMR Sensors FAQ

Operating Circuit

What is Output voltage?

With the exception of some specific products, an AMR sensor delivers binary digital output levels (H and L). Depending on the product, the sensor outputs an H or an L when switched on. See the specs sheet for details. Generally, the H-level output voltage is 90% or higher of Vcc, while the L-level output voltage is 10% or less of the supply voltage. 

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send