AMR Sensors FAQ

Characteristics

What is Hon?

Hon represents the strength of the external magnetic field strength at which the AMR sensor is switched on. 
The datasheet shows the magnetic field strength at which this product is switched on without fail under certain conditions. However, some individual units may be switched on below this figure.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send