AMR Sensors FAQ

Part Naumbers

What are the detection ranges in open/close applications? Which products do you recommend for these applications?

The detection range varies depending on the magnet used. Let us check relevant data, such as the material and size of the magnet, in each project.
We would recommend the AMRMS511 and 211 series for open/close movements as slow as those made by the hand. 

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send