AMR Sensors FAQ

Part Numbers

What is the difference between magnetic switches for open/close detection and for rotation detection?

The two types of magnetic switches detect the magnetic field in different ways. 
The open/close sensor detects the magnetic field strength, which corresponds to the distance to the magnet. 
The rotation sensor checks to see if the magnetic lines are in the same direction as its sensing direction. In doing so, it can see if the magnet is rotated or not.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send