Barometric Pressure Sensor FAQ

What is the characteristics of pressure sensor?

Advantage:                                                                                                                                             
a) Low noise, Low power 
b) Stability over temperature (<100 ppm/ °C) 
c) High sensitivity (tens of %)
d) High impedance 
e) Immunity to stress
Disadvantage:

a) Die size slightly larger
b) Needs numerical linearization


We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send