Barometric Pressure Sensor FAQ

What is the definition of Relative Accuracy?

It defines that when we change pressure between the 2 points within 800~1100hPa at temperature+25℃, the rate gap from true value would be within ±○Pa. As for Indoor navigation, it requires to reset 0 at that time and detect pressure change at"t" time accurately.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send