Inclinometers FAQ

Operating Circuit

Is it possible to decrease SCA 61T's frequency response with an additional capacitor? Is it possible for customer to make its frequency response lower by using additional electronic, e.g. high order low-pass filters?

Yes, it is possible to add active or passive filtering to the sensors output. Resistive and capacivite load on the output must be within specified limits.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send