Inclinometers FAQQIs the self test pin input DC or AC and what is the maximum input quantity?

A
DC voltage and the maximum input quantity is Vdd+0.3V (absolute maximum rating)

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.