Inclinometers FAQ

Others

What is functional form of the inclinometer output?

Inclinometers measure the effect of earth's gravity on the silicon proof mass. This is a sinusoidal function of the inclination angle. However, to get the best and most linear measurement result one should add the angular error caused by the Cross-axis Sensitivity component in the inclination plane and mounting errors.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send