Inclinometers FAQ

Others

Is there a way to save calibration data into SCA 61T/100T via SPI by customer?

Calibration data can be programmed into device memory. This feature is used during factory calibration. The re-calibration at customer site requires special agreement between Murata and customer.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send