Infrared Sensors FAQ

Characteristics

Can we use Pyroelectric infrared sensor  outside?

Yes. Please set sensor to avoid direct sunlight, air flow and wet humid. Pyroelectric infrared sensor detects temperature change by these condition. In the place of wet and humid, incorrect detection is much more occurred because optical characteristic is changed by moisture putting on lens surface and optical filter.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send