Magnetic Pattern Recognition Sensors FAQ

Operating Circuit

Precautions for circuit design

Refer to "Recommended Circuit" in the Application Guide. Since the signal level is minute, the amplification factor must be high. For the operational amplifier, the CM358 or equivalent low-noise type is recommended. For sensor output coupling capacitors, Tantalum capacitors or ceramic capacitors that generate little leakage current are recommended.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send