Magnetic Pattern Recognition Sensors FAQ

Characteristics

How wide (mm) is the maximum detecting width?

Sensors with a detecting width of 6mm or 10mm have been available from Murata. According to users' needs, we can offer custom-made models with a detecting width of 20mm or less.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send