Magnetic Pattern Recognition Sensors FAQ

Characteristics

Is it possible for the sensors to detect magnetic ink patterns printed on both the front and back of paper simultaneously from one side?

If the paper thickness is 0.1mm, when patterns on both the front and back of the paper are simultaneously detected, the signal level for the back pattern is approx. 85% of that for the front pattern. For details, refer to "Gap Characteristic" in the Application Guide.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send