Magnetic Pattern Recognition Sensors FAQ

Configurations/Material

Which polarity does the detecting surface have?

With the BS05N1 and BS05C1 types, the detecting surface functions as the S pole. With other types of sensors, it works as the N pole. The polarity has no influence on the sensors' performance (output, response, etc.). However, when the sensors read magnetic patterns, the rise of the output signal varies depending on the polarity.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send