Rotary Position Sensors FAQ

Configurations/Material

What are its dimensions and weight?

It is 12 x 11 x 2.1mm and weighs 0.4g. Please refer to this link for details.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send