Shock Sensors FAQ

Characteristics

What is the acceleration measurement resolution of the shock sensor?

Since it depends on the circuit characteristics of semiconductor amplifire in use and the generated noise, measurement resolution may vary. However, if coupled with good amplifier, the acceleration measurement resolution is about 10mG.
1G = 9.80665m/s2 in unit of acceleration. Typical 3-axis acceleration sensor is about 1-10mG.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send