Temperature Sesnsors FAQ

Characteristics

[NXR Series] What is the measurement temperature error at each temperature?

This varies with the characteristic. The temperature sensing accuracy of flagship product NXRT15XH103F serise is within ±2°C in the temperature range of -40°C to +125°C. For another characteristic, contact us.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send