Temperature Sesnsors FAQ

Configurations/Material

[NXR Series] Is this Series available in taping packaging?

The standard type is available in 5mm lead pitch taping packaging.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send