Temperature Sesnsors FAQ

Mounting

[NCP Series] Can the NCP Series be flow-soldered?

NCP18/21 Series can be flow-soldered within the range shown in the temperature-time relationship graph given below.

Allowable Flow Soldering Temp. and Time

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send