Temperature Sesnsors FAQ

Mounting

[PTFM series] What torque value do you recommend when you moust ths product with screw?

The recommended value is 4 ~8kg. In case of mounting this product with screw , please do not apply an excessive tensile stress(9.8N)
  between resin case and lead.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send