Ultrasonic Sensors FAQ

Characteristics 
Waterproof type/Open-Structure type/High-Frequency type

Is it possible to detect short distances?

It is possible to detect approximately 15cm by adjusting the drive voltage and the number of drive waves, but we believe it is difficult to detect approximately 10cm or less because the impact of reverberations cannot be eliminated entirely. 

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send