Ultrasonic Sensors FAQQWhat is the distance that can be detected? 

A
In general use of the open structure type, distances from 0.3 to 2.5m can be detected. This figure can be increased slightly depending on the drive voltage and receiver circuit gain (Murata products have been used to detect up to 4m.)

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.